PROJECT NOTES FOR ATICOMBINEDDAQFT .NET ASSEMBLY
Sam Skuce
ATI Industrial Automation

This ATICombinedDAQFT .NET assembly uses the ATI DAQ F/T C library and a hardware interface component to create
a single interface through which Force and Torque readings can be collected from the ATI DAQ F/T system.  

------------------------------------------------------------------------------------------------------
Assumptions

-The transducer is attached to six or seven sequential channels on one DAQ device, which gauge 0 connected to the
lowest numbered channel, gauge 1 connected to the next-lowest numbered channel, etc...  If the thermistor is used,
it is connected to the next-highest numbered channel after gauge 5.


------------------------------------------------------------------------------------------------------
Hardware Interface Class - ATIDAQHardwareInterface
Declaration - ATIDAQHardwareInterface.h
Implementation - ATIDAQHardwareInterface.cpp

As shipped from ATI the hardware interface component works only with National Instruments' NI-DAQmx devices.  To
work with other types of data acquisition hardware, the ATIDAQHardwareInterface software class will have to be modified.


------------------------------------------------------------------------------------------------------
ATI DAQ F/T C Library 
Function Declarations:
	xmltok_impl.h
	ascii.h
	asciitab.h
	dom.h
	ftconfig.h
	ftrt.h
	iasciitab.h
	latin1tab.h
	nametab.h
	stack.h
	utf8tab.h
	xmldef.h
	xmlparse.h
	xmlrole.h
	xmltok.h
Function Implementations:
	dom.c
	events.c*
	expatls.c
	ftconfig.c
	ftrt.c
	node.c
	stack.c
	xmlparse.c
	xmlrole.c
	xmltok.c
	xmltok_impl.c*
	xmltok_ns.c*
	* - file not included in project build (see below)
	
The ATI DAQ F/T C Library is a collection of routines for loading in calibration information from a .cal file, applying
output options, such as output units (Pounds vs. Newtons, etc.), tool transformations (to measure the forces and
torques acting at a point other than the transducer origin), and performing the matrix multiplications to transform
strain gauge voltages into force and torque data.

Note that the files which comprise the C library do not have the same compilation options as 'normal' C or C++ files in
a Visual Studio.Net project.  For one, they do not use precompiled headers (in Visual Studio.Net, right-click the file
in the Solution Explorer window, select "Properties", and visit the "C/C++"->"Precompiled Headers" section).  For 
another, the files events.c, xmltok_impl.c, and xmltok_ns.c are not included in the build at all, but they must be
in the same directory as the other files in the C library, because they are #included into other files.  To exclude
a project from the build in VS.NET, right click the file in solution explorer, select the "General Section" and set the
"Excluded from build" property.  Also, if certain functions are called from managed c++ code, they will generate linker
error 1235 in Visual C++ 2003.  To avoid this, set the "Compile as Managed" property of the file in which the function
is defined to "Not Using Managed Extensions".  To compile this particular project, ftconfig.c has to be configured in
this way.